제품이 장바구니에 추가됨
Polarizer Selection Guide
Edmund Optics Inc.

Polarizer Selection Guide

저자: Stefaan Vandendriessche

For more information on polarization read Introduction to Polarization.

Polarization is an important characteristic of light. Polarizers are key optical elements for controlling your polarization, transmitting a desired polarization state while reflecting, absorbing or deviating the rest. There is a wide variety of polarizer designs, each with its own advantages and disadvantages. To help you select the best polarizer for your application, we will discuss polarizer specifications as well as the different classes of polarizer designs.

Polarizer Characteristics

Polarizers are defined by a few key parameters, some of which are specific to polarization optics. The most important characteristics are:

Extinction Ratio and Degree of Polarization: The polarizing properties of a linear polarizer are typically defined by the degree of polarization or polarization efficiency, P, and its extinction ratio, ρp. Following the formalism given in the Handbook of Optics, the principal transmittances of the polarizer are T1 and T2. T1 is the maximum transmission of the polarizer and occurs when the axis of the polarizer is parallel to the plane of polarization of the incident polarized beam. T2 is the minimum transmission of the polarizer and occurs when the axis of the polarizer is perpendicular to the plane of polarization of the incident polarized beam.

planes of polarization

(1)$$ P = \frac{\left( T_1 - T_2 \right)}{\left( T_1 + T_2 \right)} \, \, \text{and} \, \, \rho_p = \frac{T_2}{T_1} $$

The extinction performance of a linear polarizer is often expressed as 1 / ρp : 1. This parameter ranges from less than 100:1 for economical sheet polarizers to 106:1 for high quality birefringent crystalline polarizers. The extinction ratio typically varies with wavelength and incident angle and must be evaluated along with other factors like cost, size, and polarized transmission for a given application.

Transmission: This value either refers to the transmission of light polarized linearly in the direction of the polarization axis, or to the transmission of unpolarized light through the polarizer. Parallel transmission is the transmission of unpolarized light through two polarizers with their polarization axes aligned in parallel, while crossed transmission is the transmission of unpolarized light through two polarizers with their polarization axes crossed. For ideal polarizers transmission of linearly polarized light parallel to the polarization axis is 100%, parallel transmission is 50% and crossed transmission is 0%. This can be calculated with Malus’ law as described in Introduction to Polarization.

Acceptance angle: The acceptance angle is the largest deviation from design incidence angle at which the polarizer will still perform within specifications. Most polarizers are designed to work at an incidence angle of 0° or 45°, or at Brewster’s angle. The acceptance angle is important for alignment but has particular importance when working with non-collimated beams. Wire grid and dichroic polarizers have the largest acceptance angles, up to a full acceptance angle of almost 90°.

Construction: Polarizers come in many forms and designs. Thin film polarizers are thin films similar to optical filters. Polarizing plate beamsplitters are thin, flat plates placed at an angle to the beam. Polarizing cube beamsplitters consist of two right angle prisms mounted together at the hypotenuse. Birefringent polarizers consist of two crystalline prisms mounted together, where the angle of the prisms is determined by the specific polarizer design.

Clear aperture: The clear aperture is typically most restrictive for birefringent polarizers as the availability of optically pure crystals limits the size of these polarizers. Dichroic polarizers have the largest available clear apertures as their fabrication lends itself to larger sizes.

Optical path length: The length light must travel through the polarizer. Important for dispersion, damage thresholds, and space constraints, optical path lengths can be significant in birefringent polarizers but are usually short in dichroic polarizers.

Damage threshold: The laser damage threshold is determined by the material used as well as the polarizer design, with birefringent polarizers typically having the highest damage threshold. Cement is often the most susceptible element to laser damage, which is why optically contacted beamsplitters or air spaced birefringent polarizers have higher damage thresholds.

Cost: Some polarizers require large, very pure crystals, which are expensive, while others are made of stretched plastic, which make them more economical.  

 

Selection Guide Graphs Polarization

 

Selection Guide Graphs Polarization

 

Selection Guide Graphs Polarization

  

  Extinction Ratio Laser Induced Damage Threshold (LIDT) Wavelength Range (nm) Thickness Cost
Dichroic Polarizers     

High Contrast Linear Polarizing Film (XP42)

Low to Medium
Low
400 - 700
Very thin
(polymer film)
\$
High-Temperature Linear Polarizing Film (XP40HT)
Low to Medium
Low
400 - 700
Very thin
(polymer film)
\$
High Transmission Linear Polarizing Film (XP44)
Low to Medium
Low
400 - 700
Very thin
(polymer film)
\$
Commercial Grade Visible Linear Polarizing Film (XP38)
Low to Medium
Low
400 - 700
Very thin
(polymer film)
\$
High Contrast Near-Infrared (NIR) Polarizing Film
Low to Medium
Low
400 - 1600
Very thin
(polymer film)
\$$
Ultra-Broadband Near-Infrared (NIR) Polarizing Film
Low to Medium
Low
400 - 2200
Very thin
(polymer film)
\$$
High Contrast Plastic Linear Polarizers (XP42-200)
Low to Medium
Low
400 - 700
Thin (laminated)
\$
High Contrast Glass Linear Polarizers (XP42)
Low to Medium
Low
400 - 700
Thin (laminated)
\$
Circular Polarizers (CP42HE, CP42HER)
Low to Medium
Low
400 - 700
Very thin
(polymer film)
\$
High Performance Glass Linear Polarizers
Medium
Low
400 - 700
Thin (laminated)
\$
Mounted Machine Vision Glass Linear Polarizers
Low to Medium
Low
400 - 700
Thin (laminated)
\$
NIR Glass Linear Polarizers
Low to Medium
Low
400 - 2000
Thin (laminated)
\$$
Broadband Polarizers
Medium
Low
300 - 2700
Thin
\$$$
UV, VIS-NIR, and NIR High Contrast Polarizers
High
Low to Medium
360 - 1700
Thin (laminated)
\$$$
Mid-Wave Infrared (MWIR) Polarizers
Medium
Low to Medium
1500 - 5000
Thin
\$$$
Corning Polarcor™ Glass Polarizers
Medium to High
Medium to High
630 - 1160
Thin
\$$$
Reflective Polarizers     
Wire-Grid Polarizing Film
Low to Medium
Low
400 - 1200
Very thin (film)
\$
Infrared (IR) Wire Grid Polarizers
Low to Medium
Low to Medium
2000 - 30,000
Thin
\$$$
Ultra Broadband Wire Grid Polarizers
Medium to High
Low to Medium
300 - 3200
Thin
\$$$
High Contrast IR Wire Grid Polarizers
Medium to High
Medium to High
3000 - 15000
Thin
\$$$
Protective Overcoat Wire Grid Polarizers
Low
Low to Medium
400 - 700
Thin (laminated)
\$$
UV Wire Grid Polarizers
Low to Medium
Low to Medium
240 - 400
Thin (laminated)
\$$
Brewster Windows
Low
Medium to high
200 - 2200
Thin
\$ - \$\$
Birefringent Polarizers    
Wollaston Polarizers
High
High
190 - 4000
Very thick
\$$$
Rochon Polarizers
High
High 130 - 4000 Very thick \$$$
Glan-Type Polarizers
High
High
220 - 2200
Very thick
\$$$
Thin Film Polarizers     
Ultrafast Thin Film Polarizer
Low
Medium to High
750 - 1090
Thin
\$$
Thin Film Laser Line Polarizers
Medium
Medium to High
355-1064
Thin
\$$

 

Selection Guide: Dichroic Polarizers

Dichroic polarizers transmit the desired polarization and absorb the rest. This is achieved via anisotropy in the polarizer; common examples are oriented polymer molecules and stretched nanoparticles. This is a broad class of polarizers, going from low cost laminated plastic polarizers to precision high cost glass nanoparticle polarizers. Most dichroic polarizers have good extinction ratios relative to their cost. Their damage thresholds and environmental stability are often limited, although glass dichroic polarizers outperform plastic dichroic polarizers in this aspect. Dichroic polarizers are well suited for microscopy, imaging and display applications, and are often the only choice when very large apertures are necessary.

Dichroic polarizers absorb the unwanted polarization state
Figure 1: Dichroic polarizers absorb the unwanted polarization state

 

Selection Guide: Thin Film Polarizers

 Thin Film polarizers utilize a thin-film dielectric coating to separate a beam into s- and p-polarization, commonly at a 45 degree AOI. They are often specified for optimal transmission/reflection performance at laser line wavelengths. 

Selection Guide: Reflective Polarizers

Reflective polarizers transmit the desired polarization and reflect the rest. They either use a wire grid, Brewster’s angle, or interference effects. Brewster’s angle is the angle at which, based on the Fresnel equations, only s-polarized light is reflected. Because the p-polarized light is not reflected while the s-polarized light is partially reflected, the transmitted light is enriched in p-polarization.

Reflective polarizers reflect the unwanted polarization state
Figure 2: Reflective polarizers, available as cube beamsplitters, plate beamsplitters, or thin films, reflect the unwanted polarization state

 

 

Selection Guide: Birefringent Polarizers

Birefringent polarizers transmit the desired polarization and deviate the rest. They rely on birefringent crystals, where the refractive index of light depends on its polarization. Unpolarized light at non-normal incidence will split into two separate beams upon entering the crystal, as the refraction for s- and p-polarized light will be different. Most designs consist of two joined birefringent prisms, where the angle they are joined at and the relative orientation of their optical axes determine the functionality of the polarizer. Because these polarizers require optically pure crystals they are expensive, but have high laser damage thresholds, excellent extinction ratios and broad wavelength ranges.

Cystalline polarizers transmit a desired polarization and deviate the rest
Figure 3: Crystalline polarizers, such as the Glan-Taylor polarizer, transmit a desired polarization and deviate the rest, using birefringent properties of their crystalline materials

Figure 4a: Glan-Taylor Polarizers

Figure 4b: Glan-Laser Polarizers

Figure 4c: Glan-Thompson Polarizers

 

Laser-Cut Polymer Polarizer and Retarder Quote Tool

Insert main image shown at top of tool here Looking for a custom polarizer? Edmund Optics® offers custom polymer polarizers and retarders in a wide range of film types, sizes, and shapes. Products include linear and circular polymer polarizers, and retarders. To obtain pricing information for our most popular laser-cut polarizing films please enter your requirements below. If you cannot find what you are looking for please contact our product support team and we will be happy to assist you with your enquiry.

GO TO TOOL


      

 

 

 

ITOS GmbH is a division of Edmund Optics that has provided both custom and off-the shelf polarization solutions to the German and European markets since 1993. The ITOS division expands Edmund Optics' polarization manufacturing and metrology capabilities, providing customers with a wider range of standard and custom polarization optics.


References

  1. Bass, Michael, Casimer DeCusatis, Jay Enoch, Vasudevan Lakshminarayanan, Guifang Li, Carolyn MacDonald, Virendra Mahajan, and Eric Van Stryland, eds. Handbook of Optics: Geometrical and Physical Optics, Polarized Light, Components and Instruments. 3rd ed. Vol. 1. New York, NY: McGraw-Hill Education, 2010.
  2. Goldstein, Dennis. Polarized Light. 2nd ed. New York, NY: Marcel Dekker, 2003.
본 콘텐츠가 도움이 되었습니까?

 

 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
;