제품이 장바구니에 추가됨

Edmund Optics®

지식센터

 검증된 라이브러리로 240명 이상의 글로벌 엔지니어가 참여하여 만든 신뢰할 수 있는 기술 자료를 제공합니다.

필터
Search Results for: Ocean Optics (35)

Cleaning Optics

Looking for the best way to clean optics? Learn more about the different cleaning products and methods, along with tips to handle optics at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

광학 필터의 배치 방향

Don't let your optical filter performance be negatively impacted by the AOI and CHA of your light source.

바로 보기 저장된 콘텐츠 목록에 추가

Resolution과 Contrast 비교

Learn how Edmund Optics maintains optical performance across the entire image plane through this resolution and contrast comparison using our C Series FFL lens.

바로 보기 저장된 콘텐츠 목록에 추가

빔 익스팬더 선택 가이드

Not sure which beam expander will work best in your application? Check out EO's Beam Expander Selection Guide to easily compare each type at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Kinematic Movement 고찰

A Kinematic mount is classified by all degrees of freedom being fully constrained. Need a mount? Browse through the different variations at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

표면 하부의 손상

Subsurface damage in optical components can lead to increased absorption and scatter, reducing system performance.

바로 보기 저장된 콘텐츠 목록에 추가

Aspherized Achromatic Lenses

Want an inside look at Aspherized Achromatic Lenses? Learn about the advantages, composition, and aspherized process at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Telecentric Lens 크기 제어

Telecentric Lenses can grow quite large and heavy with small magnifications, as such magnifications require large front optics. Learn more at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

금속 미러 코팅

Want to learn more about metallic mirror coatings? Find information about standard and custom metallic mirror coatings that are available at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Key Parameters of a Laser System

Learn the key parameters that must be considered to ensure you laser application is successful. Common terminology will be established for these parameters.

바로 보기 저장된 콘텐츠 목록에 추가

레이저 광학의 일반 소재

Understanding the most commonly used laser optics materials will allow for easy navigation of EO’s wide selection of laser optics components.

바로 보기 저장된 콘텐츠 목록에 추가

비구면 렌즈의 불균일성과 스트렐 비율

The Strehl ratio of an optical system is a comparison of its real performance with its diffraction-limited performance.

바로 보기 저장된 콘텐츠 목록에 추가

Spherical Aberration Compensation Plates 깊게 들여다 보기

Spherical aberrations occur in any spherical optic and causes system performance to decrease. Learn how spherical aberration compensation plates can help at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

EO에서 취급하는 글래스 타입

With over 65 optical glass types readily available at manufacturing sites, EO enables quick prototyping. View the full list of glass types at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Ball Lens 이해하기

Have a question about ball lenses? Find more information about these optical components including essential equations and application examples at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

희토류 이해

Rare earth materials are used in many optics. Find an explanation, examples, and more information about rare earths at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

빔 익스팬더 테스트

Shack-Hartmann wavefront sensors are used to test the transmitted wavefront error of laser beam expanders, predicting the real-world performance of the beam expander.

바로 보기 저장된 콘텐츠 목록에 추가

광학 수차의 비교

Trying to understand optical aberrations? Check out how to identify aberrations and view examples at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Imaging Electronics 101: 이미징 시스템 성능 개선을 위한 카메라 해상도

Camera resolution is one of the many aspects contributing to the quality of your imaging system. Find key parameters and tech tips at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

USB & GigE 카메라에 전원을 공급하는 방법: 올바른 액세서리 선택하기

Optimizing your imaging system means more than just choosing the right camera. Selecting the correct camera accessories ensures optimum performance, system stability, and successful integration. This application note explains power requirements for the two most common camera interfaces, USB and GigE, details the essential and optional accessories that enable reliable power delivery, and gives expert tips for selecting the most suitable components for your imaging system.

바로 보기 저장된 콘텐츠 목록에 추가

색 수차와 단색 광학 수차

Are you looking to design or correct the optical aberation for a system? Learn more about chromatic and monochromatic optical aberations at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

구면 렌즈의 정밀 허용오차

Optical lenses require very precise tolerances. Learn more about tolerances for spherical lenses at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

High-Power Optical Coating의 복잡성

Want to know more about high-power optical coatings? Find out more about the importance, fabrication, and testing at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

가우시안 빔의 전파

Understanding Gaussian beam propagation is critical for understanding laser systems because many lasers are assumed to have Gaussian profiles.

바로 보기 저장된 콘텐츠 목록에 추가

Microscope와 Objective 이해

Learn about the different components used to build a microscope, key concepts, and specifications at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

렌즈의 기하학적 형태별 성능 비교

This comparison of the performance of aspheric, achromatic, and spherical PCX lenses in different situations reveals the ideal use cases for each type of lens.

바로 보기 저장된 콘텐츠 목록에 추가

온도 보정이 불필요한 비열화 개론

Athermal optical systems are not prone to temperature changes in an environment. Learn more about the importance of having an athermal design at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

무반사(AR) 코팅

Anti-reflection (AR) coatings are applied to optical components to increase throughput and reduce hazards caused by back-reflections.

바로 보기 저장된 콘텐츠 목록에 추가

표면 품질 이해하기

The surface quality of optical components the scattering off of its surface, which is especially important in laser optics applications.

바로 보기 저장된 콘텐츠 목록에 추가

Optical Glass

Choosing the right optical glass is important. Find out factors and properties on how to select the right optical glass at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
;