제품이 장바구니에 추가됨
In-line Telecentric Illumination for Machine Vision

In-line Telecentric Illumination for Machine Vision

저자: Thomas Stard & Rebecca Charboneau

Introduction to In-line Telecentric Illumination

In-line illumination, when paired with a telecentric imaging lens, is a powerful technique for high-precision machine vision applications that require detection of low-contrast surface features or through-hole inspection. This coaxial lighting method directs light along the optical axis of the imaging lens using a beamsplitter, enabling even, shadow-free illumination that highlights surface defects, etched marks, or transparent features with minimal specular reflection (Figure 1). Telecentric lenses further enhance this setup by ensuring uniform magnification across the field of view and eliminating perspective errors, which is critical for accurate dimensional measurements. In this application note, example images of objects with different surfaces are observed with in-line illumination. The images below were taken with the 0.69X CobaltTL Telecentric Lens using a diffuse, white spot light to minimize hot spots.

Figure 1: Optical Path of an In-line Illumination Telecentric Lens

Image Analysis and Evaluation of In-line Telecentric Illumination

Table 1:  Images of different objects illuminated by in-line illumination

It can be observed that objects with specular surfaces benefit from in-line illumination compared to diffuse objects like the shipping label (Panel C) or plastic cap (Panel B). The features on the reflective objects like the metal part (Panel D) or electronics circuit board (Panel E) are much more distinguishable with this type of illumination. In-line illumination is particularly well-suited for applications such as inspection of semiconductor wafers, detection of micro-scratches or defects on polished surfaces, verification of laser markings on metallic components, and inspection of drilled holes in PCBs or medical devices, where conventional lighting techniques may fail to provide sufficient contrast or geometric accuracy.

Conclusion: Key Takeaways for Integrating In-line Illumination into Vision Systems

In-line telecentric illumination is a critical component in precision machine vision applications where uniform, glare-free lighting of reflective or complex surfaces is required. By directing collimated light along the same optical axis as the camera, it eliminates glare and ensures highly consistent illumination, making it ideal for inspecting transparent, specular, or cylindrical parts. When high-accuracy measurements and reliable defect detection are needed, in-line telecentric lighting delivers the uniformity and optical control necessary for robust, repeatable vision system performance..

More Resources

Bill of Materials

  • Camera Used: LUCID Vision Labs Triton2™ TRT245S-MC, Sony IMX540, 24.5MP, Monochrome Camera (TRT245S-MC) (#28-874)
  • Lenses Used: Edmund Optics 0.69X CobaltTL Telecentric Lens (#15-872)
  • Light Used: CCS In-line Spot Light: Diffused Light Compact Spot Light HLV3-14SW-HU (#21-853)
본 콘텐츠가 도움이 되었습니까?

 

 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
;