제품이 장바구니에 추가됨

Is there a technical difference between a positive and a negative resolution target?

The pattern on a positive target is most often made from a reflective material, such as chrome, deposited on a clear background. Positive targets can also be referred to as reflective targets since incident light hitting the chrome pattern will reflect. The pattern on a negative target, on the other hand, is clear and the background is chrome. Negative targets, or “transmission targets”, are most often used with a backlight in order to increase contrast between the target and the background. In terms of a technical difference, both types of targets will have the same maximum resolution regardless of their reflective or transmissive construction.

본 콘텐츠가 도움이 되었습니까?
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
;