제품이 장바구니에 추가됨

Edmund Optics® Introduces Zerodur® Laser Line Mirrors for Thermal Stability in Precision Optical Systems

4/7/2025, Barrington, NJ USA   —

Minimise alignment drift and maximise beam quality with laser mirrors built for demanding thermal conditions.

Edmund Optics® has expanded its range of TECHSPEC® Laser Line Mirrors to include options manufactured with Zerodur®—a glass-ceramic substrate renowned for its ultra-low thermal expansion. Designed for integration into laser systems operating in thermally dynamic environments, these mirrors offer exceptional stability and optical performance.

For engineers working in aerospace, satellite systems, or research environments where thermal fluctuations are unavoidable, the TECHSPEC® Laser Line Zerodur® Mirrors provide a clear performance advantage. The combination of Zerodur® substrate and Edmund Optics’ high-efficiency dielectric coatings ensure minimal alignment drift, consistent beam quality, high reflectivity, and increased resistance to laser-induced damage.

Available off-the-shelf with coatings for common laser lines including Yb-doped (1030 – 1080nm), Nd:YAG (1064nm), their respective harmonics, and dual-band configurations, these mirrors are available with fast shipping for rapid system integration. Custom coatings are also available across the 248nm–40µm range, supporting a wide array of specialised applications.

With the addition of these laser-line options, alongside its existing broadband Zerodur® mirror range, Edmund Optics now offers its most comprehensive portfolio of off-the-shelf Zerodur® mirrors—designed to support a wide array of customer applications across industries.

To view these, and many more exciting new products from Edmund Optics, visit the new products page at www.edmundoptics.com.

About Edmund Optics:

With over 80 years of experience, Edmund Optics® has built a reputation as a trusted provider of high-quality optical components and solutions, serving a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D since 1942. The company employs over 1,300 people across 19 global locations and continues to expand.

As a leading optics and photonics company, Edmund Optics continues to innovate and expand to meet the evolving needs of its customers, offering two specialized solutions: a robust Marketplace for the best brands in optics and an Advanced Manufacturing service specializing in custom and volume production of precision optical and imaging components.

Edmund Optics’ Marketplace offers over 34,000 off-the-shelf products from in-house manufacturing and global sourcing. Edmund Optics serves as a one-stop shop for customers’ entire beam path, granting access to 40+ top-tier brands alongside its own high-quality optical components while continually expanding inventory to ensure that customers find the right components for their applications. With over 3 million items in stock, Edmund Optics ensures fast, reliable delivery. Its 24/7 online chat connects customers with engineers for real-time support across industries, enhancing the customer experience anytime, anywhere.

Edmund Optics' Advanced Manufacturing services include custom design, first article production, and volume manufacturing of high-quality optical and imaging components and systems. From initial concept validation to full-scale production, Edmund Optics manufactures over 2 million optical components and 175,000+ optical assemblies annually. With in-house design, manufacturing, assembly, and metrology expertise across four design centers and nine specialized factories worldwide, the company supports both high-volume and specialized manufacturing needs. An expert team of optical and optomechanical designers, project managers, and manufacturing engineers will guide customers seamlessly through every stage of their project.

www.edmundoptics.com

 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요
;