제품이 장바구니에 추가됨

Edmund Optics®

지식센터

 검증된 라이브러리로 240명 이상의 글로벌 엔지니어가 참여하여 만든 신뢰할 수 있는 기술 자료를 제공합니다.

필터
Search Results for: Laser Mechanics (18)

Reflective Laser Beam Shaping

Beam Shaping for High Power and Short Pulse Durations

바로 보기 저장된 콘텐츠 목록에 추가

레이저 어플리케이션을 위한 REFLECTIVE OPTICS

Beam Conditioning Optics for UV, IR, and Broadband Lasers

바로 보기 저장된 콘텐츠 목록에 추가

Ultraviolet Lasers

A new generation of small, cost-effective, CW ultraviolet (UV) lasers allows more applications to move to UV wavelengths for increased power and precision.

바로 보기 저장된 콘텐츠 목록에 추가

High Reflectivity Mirrors for Laser Applications

The industry standard method for quantifying reflectivity does not tell the whole story

바로 보기 저장된 콘텐츠 목록에 추가

Superpolished Optics

Superpolished optics with sub-angstrom surface roughness are ideal for precise laser optics applications

바로 보기 저장된 콘텐츠 목록에 추가

Extreme Ultraviolet Optics

Pushing Optics to the Extreme

바로 보기 저장된 콘텐츠 목록에 추가

2µm Lasers

The unique absorption properties of 2µm lasers allow them to create small and precise cuts for medical and materials processing applications

바로 보기 저장된 콘텐츠 목록에 추가

Semiconductor Supermirrors

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

단일 소재의 비구면 아크로매틱 렌즈

Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.

바로 보기 저장된 콘텐츠 목록에 추가

Ultrafast Highly-Dispersive Mirrors

Pulse Compression and Dispersion Compensation for Ultrafast Lasers

바로 보기 저장된 콘텐츠 목록에 추가

Trending Liquid Lenses in Imaging

Quickly Autofocus and Overcome Depth of Field Limitations

바로 보기 저장된 콘텐츠 목록에 추가

Non-Circular Optics for System Miniaturization

Trimming the Fat: Truncating Lenses to Shrink Systems

바로 보기 저장된 콘텐츠 목록에 추가

극초단 시스템의 열렌즈 효과 최소화하기

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

바로 보기 저장된 콘텐츠 목록에 추가

Stemmed Mirrors

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

바로 보기 저장된 콘텐츠 목록에 추가

Future of Spherical Lenses

Traditional spherical lenses are evolving due to the increasing demands of applications. Learn about the future of spherical lenses at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Trending in Optics: The Future of Optical Filters

New optical filters are being developed due to the advancements in applications and technologies. Learn more about the future of filters at Edmund Optics.

바로 보기 저장된 콘텐츠 목록에 추가

Non-Line-of-Sight Imaging

Seeing around corners is no longer science fiction thanks to ultrafast lasers and sensitive cameras

바로 보기 저장된 콘텐츠 목록에 추가

Aspheric Lens Takeover

Time to Replace Spherical Elements with Aspheric Lenses

바로 보기 저장된 콘텐츠 목록에 추가
 
영업 & 기술 지원
 
본사 및 지사별 연락처 확인하기
빠른
견적 요청 도구
재고 번호 입력 필요