Ultrafast lasers have revolutionized a number of application spaces, but optical components for these systems face a unique set of challenges that must be overcome to maintain high pulse quality and maximize performance.
Join us for a 45 minute webinar presented by Edmund Optics' ultrafast laser optics expert Tony Karam, Ph.D. to learn about the unique challenges faced by ultrafast laser systems and solutions for choosing the correct ultrafast optical components. Ultrafast laser systems feature extremely short pulse durations on the order of picoseconds to attoseconds, which are highly advantageous for an extensive range of applications including medical lasers, nonlinear imaging and microscopy, and materials processing.
At the conclusion of this webinar, participants will have a strong understanding around:
Tony Karam received his Ph.D. in Chemistry, Ultrafast Spectroscopy, and Nanotechnology from Louisiana State University. Following his graduate studies, he moved to the California Institute of Technology as a postdoctoral scholar at the Center for Ultrafast Science and Technology under the supervision of Nobel Laureate Ahmed Zewail. At Caltech, he worked on the development of ultrafast electron diffraction and microscopy for the investigation of lattice dynamics, correlated atomic motion, and structural transformation in atomically-thin materials and nanofilms. Tony is now a Laser Optics Product Line Manager in Edmund Optics’ Barrington, NJ, USA office where he has been working on the development and commercialization of optical elements and components for laser applications. He is the author of over 40 publications on ultrafast lasers, material science, and photonics.
혹은 지사별 연락처 확인
견적 도구
재고번호 입력 후 바로 시작
Copyright 2023, 에드몬드 옵틱스 코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동 풍성빌딩)