에드몬드 옵틱스는 자사 웹사이트의 기술 서비스 기능을 최적화하기 위해 자사와 제3자의 쿠키를 이용합니다. EO의 쿠키 활용 방안에 관해 확인하십시오.

  • 내 정보
  •   
Resources / 용어 정리 / W

Glossary: W

Warm-Up Time

The time required by a laser to reach a designated percentage of the final output power (typically 95%).

  See also Laser

Wavelength

The peak to peak distance covered by one cycle of an electromagnetic wave. It is inversely related to frequency. The longer the wavelength, the lower the frequency; conversely, the shorter the wavelength, the higher the frequency.

Wedge Angle

A small angle of incline between two faces in a wedge element.

White Balance

A function in cameras that allows for calibration of colors in different lighting conditions using a reference white.

Wide-Field Eyepiece

A type of eyepiece design consisting of one achromatic doublet lens and one plano-convex lens whose convex surfaces face each other. It creates a field of view greater than 50°, hence the wide-field denotation in the name. It is designed for use with high power achromatic objectives.

Wire Grid Polarizer

A type of polarizer consisting of a thin layer of aluminum MicroWires™ sandwiched between two glass windows. It reflects S-polarized light while transmitting P-polarized light and offers a higher transmission level and higher maximum operating temperature compared to glass and film linear polarizers.

Wobble

Generally defined with reference to a rotation stage, the measure of the tilting of a rotation stage's platform frequently caused by the axis of rotation not being perpendicular to the platform.

Working Distance (WD)

The distance from the front end of a lens system to the object under inspection.

Working f/#

The effective f/# of a lens, taking into consideration the magnification at finite working distances. Calculated by (1+lml)*Infinite f/#, where m is lens magnification.

Worm Gear Drive

A type of drive mechanism for rotary stages in which a worm wheel (gear) attached to the stage shaft meshes with the worm drive, whose shaft extends out of the housing. Controlled rotation of the worm shaft creates precise angular rotation of the worm wheel and stage shaft. The worm gear and shaft are matched sets and are pre-loaded to remove backlash.

WRATTEN Filter

A type of filter created by dissolving organic dyes in a gelatin material to achieve the desired spectral performance. The gelatin liquid and dye combination is then coated onto a supportive substrate until it has dried. After removal from the substrate, the film is coated with laquer for protection. Although the filters are coated, they should be handled only by the edges or in the corners to avoid damage.

  See also Filter

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging 및 laser optics assemblies, 그리고 mechanics는 EO 전문 제품의 일부에 지나지 않습니다.

에드몬드 옵틱스의 엔지니어는 최상의 솔루션을 제공할 수 있는 전문가들입니다. 기성품부터 맞춤형 설계까지, EO가 갖춘 산업 및 기술에 관한 전문적 지식으로 고객의 요건을 충족해 드립니다.

세계적인 수준의 서비스를 지역별로 제공하고자 미국, 유럽 및 아시아에 15개 이상의 지역 사무소 운영.

Edmund Optics에 연락할 일이 있으신가요? 여러분의 필요에 맞는 당사의 빠르고 친절한 서비스를 이용하십시오.

제품 견적 요청은?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×