Edmund Optics® offers three main types of cube beamsplitters: polarizing, non-polarizing, and lateral displacement. Polarizing cube beamsplitters divide unpolarized light into two orthogonally polarized beams. They are typically used in laser beam separation/combination applications, laser mirrors for beam steering, and semiconductor and photonics instrumentation. Non-polarizing cube beamsplitters divide light evenly, regardless of polarization. They are used in laser mirrors for beam steering, optical interferometry, and biomedical instrumentation. Lateral displacement beamsplitters split incident light beams into two displaced, parallel beams; they can be thought of as a sub-type of polarizing cube beamsplitters since the displaced beam is S-polarized while the other is P-polarized.
Polarizing | Non-Polarizing | Lateral Displacement |
---|---|---|
혹은 지사별 연락처 확인
견적 도구
재고번호 입력 후 바로 시작
Copyright 2023, 에드몬드 옵틱스 코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동 풍성빌딩)