EO Imaging: Telecentric Lenses versus Hypercentric Lenses
Join EO's Nick Sischka, Director of Imaging, as he inspects pipes for various defects using the TECHSPEC Telecentric Lens versus the TECHSPEC Hypercentric Lens. In this demo, discover how different optics can yield dramatically different results in imaging systems. How can we help with your next inspection application?
My name is Nick Sischka. I am a Machine Vision Engineer at Edmund Optics. The demo I am showing today is a demo on some of our machine vision capabilities that we have, we are showing off. Keeping in the theme of our Trade Show right now, which is "Where Do Your Optics Go?". One of the places that optics can go is in inspection, inspection lines, and what we are doing right now is showing several different pipes made out of several different materials, different inter-diameters, containing different features. We are showing a telecentric lens with collimated illumination, which shows very very very accurately any burrs or occlusions or anything that is going to show up coming from these pipes that are errors. What that doesn't show you is where the actual occlusion is located, how far down the pipe it is, whether or not it's endemic throughout the entire length of the pipe. And so what we can do to show that is use a hypercentric lens which utilizes slightly different optical converging rays and what you can actually do is use this as a borescope. So, what you can see is some of the weld seams that go down the inside of the pipe. We can see some of the bored holes that come out, whereas on the telecentric lens they show up as burrs but you can't really tell what they are. Looking at them with the hypercentric you can see that it is a hole that goes all the way through. And really just showing off some of the more niche products that we have for machine vision that are not used every day. Again, my name is Nick Sischka. I am a Machine Vision Engineer at Edmund Optics, and if you would like more information on this, please visit us on the web at www.edmundoptics.com/.
혹은 지사별 연락처 확인
견적 도구
재고번호 입력 후 바로 시작
Copyright 2023, 에드몬드 옵틱스 코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동 풍성빌딩)