Can You See Beyond the Visible?
A large number of applications that are difficult or impossible to perform using visible light are made possible, with superior results, using short-wave infrared (SWIR) imaging thus enabling the user to "See Beyond the Visible." Unlike mid-wave infrared (MWIR) and long-wave infrared (LWIR) light, which is emitted from the object itself, SWIR is similar to visible light in that photons are reflected or absorbed by an object, providing the strong contrast needed for higher resolution imaging. Ambient star light and background radiance (nightglow) are natural emitters of SWIR and provide excellent illumination for outdoor or nighttime imaging including imaging though fog, haze and water vapors.
Most Popular SWIR Imaging Applications
- Electronic Board Inspection
- Solar Cell Inspection
- Identifying and Sorting
- Produce Inspection
- Surveillance
- Anti-Counterfeiting
- Process Quality Control
ROLL OVER to See SWIR Image
Figure 2a: Visible Imaging of Red Apple. Notice the Apple Looks Perfectly Red with Visible Imaging. Defects are Not Easily Discernable.
ROLL OVER to See SWIR Image
Figure 2b: SWIR Imaging of Red Apple. Bruising is Clearly Evident on the Apple with SWIR Imaging. It is Easy to Inspect Any Defects on the Skin.
ROLL OVER to See SWIR Image
Figure 3a: Visible Imaging of Baby Powder Bottle. Notice the Bottle Looks White and Glossy with Visible Imaging. The Powder within is not Discernable at All.
ROLL OVER to See SWIR Image
Figure 3b: SWIR Imaging of Baby Powder Bottle. The Bottle is Transparent to SWIR Wavelengths. It is Easy to See the Amount of Powder Within.
ROLL OVER to See SWIR Image
Figure 4a: The Last Judgement by Jan Provost and imaged in the SWIR waveband by the Detroit Institute of Arts details the artist's original intention by carefully examining the underdrawing which lies beneath the paint film. Image copyright by Detroit Institute of Arts. Used with permission.
ROLL OVER to See SWIR Image
Figure 4b: One can see 10 trumpets underneath the archangel versus the 5 trumpets that were actually painted. The placement of the painted trumpets appears to have necessitated a reposition of the sailing vessel. The toes on top of the globe were also not painted in the same location as the original underdrawing. Image copyright by Detroit Institute of Arts. Used with permission.
ROLL OVER to See SWIR Image
Figure 5a: Bountiful Fruit painted by Philadelphia artist Nicole D. Tartaglia details the planning process of an artist when creating an oil painting. By examining the painting in the SWIR waveband one can follow the artist's thought process from initial sketch to painting and refinement of finished work.
ROLL OVER to See SWIR Image
Figure 5b: As you can see, the painting originally included bananas and a frame that were omitted from the final image. Along the lower right there appears to be blotches of paint not seen in the visible waveband. Perhaps the artist began painting the background with different materials or changed her mind and touched up the painting at a later date.
Edmund Optics is Your SWIR Imaging Expert
Capable of manufacturing and assembling in volume to the highest standards, Edmund Optics is experienced in designing, manufacturing, and coating SWIR imaging lenses. Edmund Optics offers lens assemblies designed with glasses that are optimized for performance in the SWIR spectrum, and our SWIR anti-reflection (AR) coatings are specially designed for maximum transmission of SWIR wavelengths.
It is essential to use a lens that is both designed and coated for the SWIR wavelength band. Using a lens designed for the visible spectrum will result in low resolution images and higher optical aberrations.
Start Shopping
SWIR Imaging Lens Specifications
- Designed for Superior Image Quality and SWIR Wavelengths
- AR Coated for R<0.5% @ 800 - 1800nm
- Supports up to 25.6mm Sensors
Need Expert Advice?
Contact us today to get in touch with an applications engineer to discuss your requirements.
Related Resources
Edmund Optics makes it easy to find the right product for your application. You can learn more about SWIR technology and determine if SWIR imaging lenses are well-suited for your application.
혹은 지사별 연락처 확인
견적 도구
재고번호 입력 후 바로 시작
Copyright 2023, 에드몬드 옵틱스 코리아 사업자 등록번호: 110-81-74657 | 대표이사: 앙텍하우 | 통신판매업 신고번호: 제 2022-서울마포-0965호, 서울특별시 마포구 월드컵북로 21, 7층 (서교동 풍성빌딩)